This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Application development

Hi all, I am working on Pandboard ES(omap4430) with ubuntu 12.04. I need to create applications such as acquiring data from serial port and show it on LCD screen , use GPIO 's when required , etc., ( a simple GUI application with embedded drivers (serial) ) .Is it possible with CCS ? or do I need to go with eclipse or netbeans ?? if its possible with CCS how do I get started . Currently I am having a flash card of 8gb that is running the OS. I dont have a JTAG debugger. Thanks in advance. This is my first application on a Linux platform . Any help is much appreciated.