I'm using CCS 5.1 from the installation DVD for TMDSEVM6678. The suite is up and running, and I've successfully debugged the EVM using the on board USB JTAG emulator (TI XDS100v1 USB Emulator). I purchased a Blackhawk XDS560v2 System Trace emulator to give me more debugging speed and power, but it does not show up in the Connection List under CCS.
First, I tried to grab a driver from within the CCS installation folder, because Blackhawk claimed that drivers were included in CCS 4.x and higher. Windows could not find a driver, so I ended up using the driver that came on the CD from Blackhawk. It shows up properly in device manager:
But does not show up when I boot CCS and try to define a new target configuration:
Any help would be greatly appreciated.