I am starting to work with 28035 Experimenter Kit. First thing was following steps on System Framework Overview pdf file and could get FlashingLed example running without problems.
Checked example results and closed CCS4 when finished working.
Next time I tried to run Flashing Leds example, I opened CCS4 on the corresponding workspace.
Tied to connect to Target hitting debug button but cannot connect to Target, and I get the error message:
Error connecting to the target:
Error 0x80000200/-1142
Fatal Error during: OCS,
Processor blocked debug accesses. An operation was attempted while
the CPU was in a non-debuggable context. To continue to honor the debug
context, press Cancel. To force debug access, press Rude Retry.
tried several times checking Debuggging configuration with no success
After checking some other answers in this forum, I understand this problem might be related with Real Time Mode debugging but could not get the Target running again. Always getting same message.
Look forward to getting an answer which helps me get this going.
Thanks