After update to CCS 5.2.1.00018 the descriptions of the errors, warnings and remarks contain only the ID (e.g. "#880-D" ).
If deactivating the verbose diagnostic the description contains the string "#880-D parameter "MyVar" was never referenced".
Additionally the "problems" window is not cleared automatically. Not sure if this is a bug or a feature... :)
Anybody else?