This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Cannot install CCS v. 5.2

Hello,

I have tried to install CCS versions 5.2.0 and 5.2.1 with no success. I downloaded the offline installer because I thought there might be issues with going through the company proxy server, but the installation still fails because it can't connect to the download server (not sure why it's trying to connect with the offline installation).

I'll preemtively answer the standard questions:

- did you redownload in case of corruption. yes -- even tried several versions
- did you turn off antivirus -- yes
- did you unzip the installer first -- yes
- did you use only directories with no spaces, accented or special characters -- yes
- did you have full permissions and avoid the program files directory -- yes
- did you fully remove the previous installation? -- there was no previous installation

The zipped InstallJammer ccsv5 directory is attached.

The system OS is Windows 7 64 bit.

Thanks for any help you can provide,

Dan

1325.ccsv5.zip