Hi, all:
when i use the jpeg encode codec with C6678, i have a problem.
The problem is when i load the .out to the C6678, i can not load it. After a while, the console in the ccs says :
C66xx_0: Power Failure on Target CPU
C66xx_0: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging.
when the ccs is loading the .out, i stop it, it stoped at the function __TI_decompress_rle_core().
Before that i use CCS5.0.1.201105110900 and C6678, it did not have that problem.
could anyone tell me what the problem is and how to solve it ?
my environment: CCS:CCS5.1.1.00031 JPEG ENCODE codec:C66x_jpegenc_02_02_00_01_ELF
thanks.
qbliu