Hello,
I have a problem after updating to CCS5.1.0 to CCS5.2.1. I use CCS only for MSP430
The compiler version is set form 4.0.0 to 4.1.1
In the current project all system included functions are displayed as warning.
See screenshot ->assert function
How can I fix this bug without resetup of the project?
Best regards Silvester Mueller