This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS 5.2: Where are Debug Loading options?



Hello,
I'm switched from CCS V4 to V5.2. Everything runs smoother and Grace is a real help.

However as I start testing our own FW update functions I wand to start the debugger without loading FW into the memory. On V4 there was a section CCS Debug > Debugger > Loading options with the option to "Load symbols only".

I can not find this option on CCS V5.2. Please help.

Guenther

  • Guenther,

    There are several ways you can do this in v5.x. A couple of them are:

    First, you can launch the debug session from the right context menu ("Launch selected configuration") from the target configuration view. When connected to the target, you can Run->Load menu or the equivalent toolbar option.

    Another way is to edit the launch configuration: pull down the bug button, and select "debug configurations ...", select the "program" tab and change the load options.

  • Hi Andy,

    Yes, that is what I was looking for.

    Regards
    Guenther