Other Parts Discussed in Thread: CCSTUDIO
The <ccs root dir>/ccsv5/ccs_base/scripting/bin/dss.sh script is broken and therefore loadti can not be run on the latest CCSv5 using a linux host.
I could not find a way to pass loadti params via com.ti.ccstudio.apps.runScript
com.ti.ccstudio.apps.runScript does take an option called -dss.rhinoArgs but the arguments passed on it are consumed by rhino instead of being passed to loadti script.
@ ../../../DebugServer/../../eclipse/eclipse -nosplash -application com.ti.ccstudio.apps.runScript
flxInitLoad: client has not been protected.
flxInitLoad: client has not been protected.
Usage:
eclipse -noSplash -data "<workspace_dir>"
-application com.ti.ccstudio.apps.runScript
[<options>]
where options include:
-dss.script <file>
Absolute or relative path to the script file (optional).
Relative paths will be resolved based on the current working-directory.
-dss.rhinoArgs "<args>"
Additional arguments to be passed to the Rhino interpreter (optional).
(use backslash '\' to escape all double-quotes in <args>).
-dss.debug
Launch the Rhino Debugger to step through the script (optional).
Defaults to 'false'.
-ccs.args <file>
File containing any extra arguments (optional).
-ccs.help
Print this help message.
If there is no way to pass paramaters then I suggest changing dss.sh to call rhino the legacy way (i.e. java -DXPCOM.RUNTIME=$DEBUGSERVER_ROOT/linux org.mozilla.javascript.tools.shell.Main)
Thanks,
Carlos