This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to unlock chip using loadti in CCS V5



I want to flash my device using loadti but not CCS.

But the chip is security by the password and I cannot earse the flash.

Can anyone konw how to unlock the device from loadti, thanks a lot

Available options:
 
  -a,   --async-run  Run the specified executable and return without halting

  -b,   --init-bss-section[=VALUE] Initialize .bss section to specified value, or 0 if  value is omitted
 
  -c,   --cfg-file=CONFIG_FILE     Target setup config file
 
  -h,   --help   Print help

  -l,   --load   Load program only

  -mlr, --mem-load-raw="PAGE,ADDR,FILE,TYPE_SIZE,BYTE_SWAP"      Load binary data file on host to target

  -mld, --mem-load-dat="PAGE,ADDR,FILE,LEN"  Load *.dat file on host to target

  -msr, --mem-save-raw="PAGE,ADDR,FILE,LEN,TYPE_SIZE,BYTE_SWAP" Save data from target memory to binary file on the host

  -msd, --mem-save-dat="PAGE,ADDR,FILE,LEN,IO_FORMAT,APPEND"
      Save data from target memory to *.dat file on the host

  -n,   --no-profile Do not perform basic application profiling (total
      cycles)

  -q,   --quiet   Quiet mode (only C I/O messages to the console)

  -r,   --reset   Reset target before run

  -s,   --stdout-file=FILE
      Save C I/O to specified file

  -t,   --timeout=VALUE Overall scripting timeout value (in milliseconds)

  -v,   --verbose  Print informative messages during execution

  -x,   --xml-log=FILE Generate specified XML log file
    -@,   --options-file=FILE