I am using CCS Version: 5.2.1.00018 with Windows 7 and the "Check for Updates" found none.
I have an assembler only project targeting the MSP4304152 on a custom board.
When I start the debugger I see the "No source available" message in the source pane. The debug window shows the code and even the path to the .s43 file. but can't match this up to the assembler code. I checked the various forums and this has been discussed in the past and the implication was that a fix was in the works.
I have debug turned on, and even tried the secret .asmfunc directive to no avail.
thanks,
James