Hi All,
I met a problem in using CCS5.
I got two CCS5 projects on hand, one can successfully compiles, other fails with error.
Then I compare the .cproject file, I find difference in it.
Then I add that line of XML code, the failed project now can compile.
But I still don't know the corresponding position in the project property settings.
My question is: is there any tips to map the .cproject file to the visual setting way?
I tried to modify via the visual way, then check what was changed in the .cproject file.
But still can not find the corresponding position for the line 159 in .cproject in the zip file.
Your help is quite appreciated!