This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Interfacing TMS320C6711 DSK with CCS v4

Other Parts Discussed in Thread: CCSTUDIO

Hi! I have got the TMS320C6711 DSK board. I want to interface this wih CCStudio V4. I would like to know where do I find the drivers for this board. And I would like to know how do I interface this board with CCSv4, as there is no inbuilt support for it in CCSv4. Any guidance would be of great help. Thanks In Advance

  • Hi Gajendra,

    that I am aware this device is supported in the lateste CCSv4 production release.  In fact I just created in v4 a project for a generic C67xx device.  Have you tried that?  What CCS version are you using?

    Best Regards,

    Lisa

  • I am using CCS v4.1, and I have the board DSK  C6711, with parallel port emulator. And when I am trying to connect DSK C6711 using CCSv3.1, I am getting the following error message: - 

                  Your Code Composer does not support the connected target.

                   Device driver name: "C:\CCStudio_V3.1\drivers\sdgo6x.dvr"

    And the system configuration that was set is:-

                   DSK6711 via XDS510 PP Emulator

     

     

  • Hi Gejendra,

    is there a specific reason you are trying v3.1?  Have you tried updating your v3.1 to v3.3?  Are you trying v3 or v4?  Are you plugging the board directly in or using a different emulator in between?  What OS are you using?

    Best Regards,
    Lisa

  • Hi! Lisa

      -  I wanted to interface it with CCSv4.1 but couldnt, thats why wanted to check with CCSV3.1.

      -  I have not tried upgrading it.

      -  Yes I am using V3.1 & V4.

      -  I am plugging the board directly via parallel port.   

      - I am using Windows XP professinal  S3 

               Can you please let me know where do I find the driver for this board, or any other information that would be

    helpful.

         Thanks in Advance

     

     

  • Hi Gajendra,

    what do you mean it didn't work with v4?  What error do you get/issue do you see?  Lets see if we can't get you up and running there.

    Best Regards,

    Lisa

  • Hi Lisa

    I am having same problem.

    I want to connect my DSK 6711 through parallel port. and run it using ccs v4

    Can you please tell me step by step procedure of code composer studio setting.

    regards

    shahid khan