This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS 5.2.1 Error

I Installed CCS 5.2.1.00018.  When I execute it i get the follwing error : "Could not open the editor: No editor descriptor for id com.ti.common.ui.cmdFileEditor".  Can you please tell me how I can fix this.

 

Thanks,

Greg

  • Hi Greg,

    may I ask a few further details

    - is this a fresh installation

    - what OS are you using

    - have you always had this message on startup

    - could you please send the contents of your installjammer registry directory (under program files or program files(x86))

    - have you been sure to unzip the installer first and use directories with no accented/special characters or spaces

    Best Regards,
    Lisa

  • Hi Lisa,

    So the problem has changed.  Here is the problem i am having now.  I have migrated from v5.1 to v5.2.1.00018 on windows.  When i try to build my porject it builds but I get the following Message:

    "This project was created using a version of compiler that is not currently installed: 6.0.2 [C2000]. Another version of the compiler will be used during build: 6.1.0. Please install the compiler of the required version, or migrate the project to one of the available compiler versions by adjusting project properties.”

    Can you please help me address this message?

     

    Thanks,
    Greg

  • Hi Greg,

    unless you need the specific compiler version used with the project, feel free to accept this message and migrate your project to the newer compiler version.

    Does this help clarify things for you? 

    Best Regards,
    Lisa

  • Hi Lisa,

    It does help me know that nothing is wrong however I am unclear how to migrate to the new complier.  Do you have some instructions on that?

     

    Thanks,

    Greg

  • Hi Greg,

    if the pop up with that message does not give you the option/do the migration automatically you can go to Project->Properties->General.  In this tab you should see the compiler version used/have the drop down selection for it available.

    Please keep us informed.

    Best Regards,

    Lisa