I just bought a TMS320C6713DSK. I have CCS V5.2 installed on my Windows System 7 machine for MSP430 development. I installed the CCS V3 that comes on the DSK disk. From what I see on ti's website, there are issues about the drivers and System 7. Issues which I certainly have. So I imported one of the examples that came with the V3 into a V5.2 workspace. Now, no surprise, CCS v5 is complaining that I don't have a license for the C6000's. I have been using the free version for MSP430 design.
Is there a license that comes with the DSK? I looked in the V3 installation for a license file, but didn't find one. I wouldn't expect a license file for V3 to work with V5 anyway. What do I do?
Kent