hi,
I am using aF28027 Piccollo Control Stick to control a Buck Converter.
I am using the digital power template.
I have a reference Value, which determines the output voltage required.
I am observing the ADC output (as i increase my input voltage) ,
and the controlled duty ratio output via the watch window- with real time mode (polite and continous refresh).
When the ADC output is less than the reference value, the watch window works fine.
But when the ADC output equals the reference value (feedback voltage reaches the setpoint desired value), the watch window freezes.
Although the piccollo continues working well by controlling the buck, the watch window variables freeze and dissapear after a minute or so.
Even if i rduce the ADC output below the reference, nothing happens.
What could be happening in CCS 4.2.3 ? Is there something that needs to be activated so that the watch window can display the variables at all times?