This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello everyboby:
I build my project but it gennerate a error that "_mpy32ll(int, int) F:\\pede0809change\\pds_lib\\Debug\\pds_lib.lib " undefined symbol first referenced in file , but I has beem add " #include "IQmath_inline.h" " into file and add libarary "IQmath_c64x+.lib" to my project . so I do not find where undefined symbol "_mpy32ll"。
Thanks !
chen an
Hi ki:
I has been add rts64plus.lib to project but generate a new error ,
So how to solve this problem! please help.
Best regards to your !
chan an
------------------- dm6437_evm_video_st_sample.pjt - Debug ------------------- [Linking...] "C:\CCStudio_v3.3\C6000\cgtools\bin\cl6x" -@"Debug.lkf" <Linking> >> error: symbol _c_int00 is defined multiple times: boot.obj (C:\\CCStudio_v3.3\\C6000\\cgtools\\lib\\rts64plus.lib) and boot.o64P (C:/CCStudio_v3.3/bios_5_31_07/packages/ti/bios/lib/bios.a64P) >> error: symbol __stack is defined multiple times: boot.obj (C:\\CCStudio_v3.3\\C6000\\cgtools\\lib\\rts64plus.lib) and boot.o64P (C:/CCStudio_v3.3/bios_5_31_07/packages/ti/bios/lib/bios.a64P) >> warning: creating output section .template without SECTIONS specification >> warning: creating output section .sysmem without SECTIONS specification >> warning: creating output section .IRQ_LoadVecs without SECTIONS specification >> warning: creating .sysmem section with default size of 400 (hex) words. Use -heap option to change the default size. >> error: errors in input - ./Debug/dm6437_evm_video_st_sample.out not built >> Compilation failure Build Complete, 4 Errors, 4 Warnings, 0 Remarks.
Didn't realize you are using a BIOS project. The issue is that some symbols are defined twice. Are you trying to build some example or is this a custom project?
Hi Ki:
My project is a custom project, I used bios is "bios_5_31_07" , dependent project is pds_lib.pjt , ative project is dm6437_evm_video_st_sample.pjt,
I add run time libarary that generate a new error
if I don't add runtime libarary ,it generate other error:
so , how to do this!
Best Regards!
chan an