Other Parts Discussed in Thread: OMAPL138
Hi,
I am using SpectrumDigital XDS560V2 STM for debugging OMAPL138 chip. Sometimes it would take a significant amount of time for content to be loaded into the device (and memory) and the progress bar increments slowly in steps like 13%, 16%, …, 97%, 100%. Much time is wasted in this process.
I have already configured “Target configuration” to use “Automatic with faster 35.0MHz limit”. If I set “TMS/TDO Output Timing” to “Rising edge allows faster TCLK” instead of the “Falling edge is JTAG standard”, then the connection would fail. So I reverted this option back to the default “Falling edge is JTAG standard”.
Is there any other option to make the loading time shorter?
Paul