This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problems using project build from the command line.

Other Parts Discussed in Thread: CCSTUDIO

C:\ti\ccsv5\eclipse\eclipsec.exe -nosplash -application com.ti.ccstudio.apps.projectImport -ccs.location U:\dspsrdc_csa\emeter\dsp_c28x\G3\proj\G3_mac\g3_plc_aes_f2806x

I get the following error.

  !ERROR: Import failed for project 'g3_plc_aes_f2806x' because its compiler definition is not available. Please install the C2000v6.1 compiler before importing this project.

We still use the CCSv4.2 compiler for our code because of difficulties with the CCSv5.1 compiler.

Does this mean that I will be unable to use the command line for builds?

  • Which specific version of CCSv5 are you using? Are you sure the project you are importing is a "CCS project" and not a standard Eclipse project?

    Are you able to import the same project through the CCS GUI rather than via command line?

    What versions of compilers do you see listed under Window->Preferences->Code Composer Studio->Build->Compilers? CCS 5.2.x should already have compiler v6.1.0 for C2000 and what that version I wouldn't expect this error to appear.

  • I am using 5.1.1.00031

    From the GUI the import works fine. (Import existing Eclipse project)

    This fails from the command line.

    eclipsec -noSplash -data C:\Users\x0183614\workspace_v5_prime_int_z -application com.ti.ccstudio.apps.projectImport -ccs.location U:\dspsrdc_csa\emeter\dsp_c28x\PLC_AppBoot

      !ERROR: Import failed for project 'PLC_AppBoot' because its compiler definition is not available.
    Please install the C2000v6.1 compiler before importing this project.

    It would appear that I have the compiler installed.

    under a C2000 tab discovered tools

    ti v6.1.0A11101

    Any other ideas?

  • Bill Etcheverry said:

    From the GUI the import works fine. (Import existing Eclipse project)

    This fails from the command line.

    Is the same workspace being used in both cases, (ie) when imported using GUI and using command line? If not, can you try from command line in the same workspace that works with GUI?

  • Additional information.  The project import seems to be order dependent.  Starting with a clean workspace,

    Z:\dspsrdc_csa\emeter\dsp_c28x>eclipsec.exe -nosplash -data C:\Users\x0183614\workspace_v5_prime_int
    _z -application com.ti.ccstudio.apps.projectImport -ccs.location v:\dspsrdc_csa\emeter\dsp_c28x\PLC_
    AppBoot

    --------------------------------------------------------------------------------
    Importing project from 'v:/dspsrdc_csa/emeter/dsp_c28x/PLC_AppBoot'...

      !ERROR: Import failed for project 'PLC_AppBoot' because its compiler definition is not available.
    Please install the C2000v6.1 compiler before importing this project.

    This import failed.  But the following sequence works.

    Z:\dspsrdc_csa\emeter\dsp_c28x>eclipsec.exe -nosplash -data C:\Users\x0183614\workspace_v5_prime_int
    _z -application com.ti.ccstudio.apps.projectImport -ccs.location v:\dspsrdc_csa\emeter\dsp_c28x\prim
    e\proj\prime\prime_iec432_flash

    --------------------------------------------------------------------------------
    Importing project from 'v:/dspsrdc_csa/emeter/dsp_c28x/prime/proj/prime/prime_iec432_flash'...


    Done!

    Z:\dspsrdc_csa\emeter\dsp_c28x>eclipsec.exe -nosplash -data C:\Users\x0183614\workspace_v5_prime_int
    _z -application com.ti.ccstudio.apps.projectImport -ccs.location v:\dspsrdc_csa\emeter\dsp_c28x\PLC_
    AppBoot

    --------------------------------------------------------------------------------
    Importing project from 'v:/dspsrdc_csa/emeter/dsp_c28x/PLC_AppBoot'...


    Done!
    Job found still running after platform shutdown.  Jobs should be canceled by the plugin that schedul
    ed them during shutdown: org.eclipse.core.internal.refresh.PollingMonitor
    Job found still running after platform shutdown.  Jobs should be canceled by the plugin that schedul
    ed them during shutdown: org.eclipse.core.internal.refresh.PollingMonitor

    Any ideas?

    The "Job found still running..." comment changes but doesn't appear to bother anything.

  • Hi Bill,

    This problem has been fixed in CCSv5.2.1, which is already available for download (problem tracked by SDSCM00044275: Headless import: cannot import a project with created with newer compiler).  

    Please give that a try, and let us know.

    Thanks,

    - Baltasar