Other Parts Discussed in Thread: TMS320C6727, SPRC203
Hi,
I'm using PADK (TMS320C6727) and I want to boot up from flash. When compiling example "SwitchesAndLeds" in sprc203 provided by TI, I got following warnings:
<Linking>
"E:/padk/sprc203/TMS320C672xxBootUtils/TMS320C672xxBootUtils/Examples/Padk_examples/flashBoot/SwitchesAndLeds/TISecondaryBootPadk.cmd", line 80: warning #10068-D:
no matching section
"E:/padk/sprc203/TMS320C672xxBootUtils/TMS320C672xxBootUtils/Examples/Padk_examples/flashBoot/SwitchesAndLeds/TISecondaryBootPadk.cmd", line 81: warning #10068-D:
no matching section
'Finished building target: E:/padk/sprc203/TMS320C672xxBootUtils/TMS320C672xxBootUtils/Examples/Padk_examples/flashBoot/SwitchesAndLeds/SwitchesAndLeds/../Debug/SwitchesAndLeds.out'
the related code snippets in the linker cmd file are:
.TIBootStrap {.+= 4;} load = 0x10000000
.TIBoot { *(.TIBoot) // line 80
.\TISecondaryBootPADK.obj(.switch) // line 81
} load = 0x10002E00,
LOAD_SIZE(_TIBOOT_SEC_SIZE),
RUN_START(_TIBOOT_SEC_RUN_ADDR)
I used ofd6x.exe to see the sections in TISecondaryBootPADK.obj:
As shown in the picture, there is a section ".TIBoot" and two subsections ".switch:_TISecondary..." in that obj file, but the linker just cannot find them.
Why this happens? The version of compiler is 7.3.7, CCS version 5.2.1.00018.
Thanks for any suggestions.