This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

"Process CIO error" while loading the program in C6727 dsp

Trouble Removing Breakpoint with the Action "Process CIO" at 0x100104a8:
Error 0x80000008/-1060
Fatal Error during: Break Point,
An unknown error prevented the emulator from accessing the processor
in a timely fashion.
It is recommended to RESET EMULATOR. This will disconnect each
target from the emulator. The targets should then be power cycled
or hard reset followed by an emureset and reconnect to each target.


Sequence ID: 8
Error Code: -1060
Error Class: 0x80000008

This is the error i get while loading the program onto C6727 DSP. I am using XDS510 USB emulator.

CCS 3.3.32 used.

Please help me in knowing what is the cause of this error.

Anushree