Hi All,
Code Composer 5.2.1.00018
Windows 7 64 bit
Java Version 7 update 5 (build 1.7.0_05-b06)
I'm debugging a small issue with the sizeof() function and noticed that there is an issue with the memory renderer. In the following examples the column width is changed from 10 bytes to 11 bytes. It appears that the assessment of the lengths of uDS20_Config and gateHwi_StateMachine_Lock_Handle change.
10 byte column width
11 byte column width
Can anyone shed any light on this?
Cheers, Kirem