Other Parts Discussed in Thread: TMS320F28335
Hi,
We're in the process of writing a custom host side UART boot-loader that will run on a Linux host. We have a C5535 eZdsp kit with an on-board xds100. Would we be able to access the USB virtual com port on the XDS100 (port B) from Linux? I assume we need the XDS100 drivers but from the searchig I've done so far, I haven't found the XDS100 drivers for Linux as stand-alone. We want to avoid installing CCS on our linux machine just to get XDS100 drivers. I'm also not sure if we do install CCS if we can access the virtual com port.
Thanks