This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Start the receive of ETB-based trace automatically.

Hi there,

I can collect ETB-based trace of my DM365 HW.

How to setup CCSv5 such that it AUTOMATICALLY starts the receive of ETB-based trace upon DM365 is powered on ?

Thanks & regards,
Yulin,

  • Yulin,

    When the device is powered off CCSv5 cannot be connected to it; therefore you can't collect trace data at this point. Even if ETB could be activated at power up time, the ETB data collection is circular and therefore previous data would be overwritten when the trace buffer reached its limit.

    What people usually do is insert a forever loop at the very beginning of the boot code, which allows time to connect CCS to the device and then debug the boot process. That would also allow connecting to the ETB to collect trace data.

    Hope this helps,

    Rafael

  • Rafael,

    Yes, IF this is a issue that occurs every time after the device is released from reset.

    However, the issue (crashed somewhere in UBL) I faced happens less than 1 in 100 rounds of reset stability test.
    (DM365 triggers a HW reset after it leaves UBL and enters the test code)