Hi,
I recently upgraded to v5.2 since it solved a few outstanding issues for me. However, this new version has a bug. Whenever I compile a project with an error, it shows
up in the errors window. After I fix and hit rebuild, the console window shows that the build was successfully (hence the error resolved) but the problems window keeps showing the same errors as if they were never solved. This is quite annoying and confusing. The only solution is to do a clean and then rebuild everything, which takes time.
Is this a known issues? Any idea when it'll be resolved?
Regards,
Gustavo