This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Debugging WinCE BSP with XDS100 & CCS5.2

Hello,

I am quite new in the topic, so please bare with me. I have been searching for weeks in the web and no dice sof far. Is there any way at all to debug the BSP code created with Microsoft toolchains using the XDS100 emulator? The only decent tool that i found that talks to XDS100 is CCS, but unfortunately it cannot hook up with the code compiled and linked with MS toolchains.

Most probably the issue is the ELF file format vs. COFF format. Is there any way what so ever to debug Windows using XDS100? If so, pointers to right direction would be extremly appreciated.

Thanks in advance.

  • Hi,

    Unfortunately you have a very unusual request and therefore we haven't used CCS with WinCE for debugging.

    If the WinCE BSP binaries are in ELF format and they are built with full symbolic debug information, then CCS (Eclipse) has a great chance to load the debug symbols to help debug the BSP. The setup procedure would be very similar to what is shown in the Stop Mode debug at the page below, or in the u-boot page:

    http://processors.wiki.ti.com/index.php/Linux_Debug_in_CCSv5

    http://processors.wiki.ti.com/index.php/U-boot_Debug_in_CCSv5

    However, if the binaries are in a different format or in a heavily modified ELF, then I suspect you may have trouble making CCS properly understand the binaries. I really don't think that is the case, though.

    In any case, I am not aware of any additional details apart from what I send above. The page below also contains additional details regarding the BSP itself, including debugging, but I could not find anything related to CCS.

    http://processors.wiki.ti.com/index.php/WinCE-BSP_ARM-A8_User_Guide

    Hope this helps,

    Rafael

  • Hello,

    Yes, it helped me forward a bit. From the document you provided, I understood that there is no way to debug the WinCE bootloader, at least with XDS100. Which is a shame. One option is ofcourse to use Linux bootloaders that will load the CE kernel, but for some unknown reason it feels kind of unnatural for me.

    The whole problem started from the fact that the CE bootloader does not even reach the phase, where serial initialization takes place, therefore serial debug is out of question. I hoped to debug the bootloader with JTAG and hoped that XDS100 would do the trick. I was mistaken. My bad. Lesson learnt.

    Thank you very much for prompt answer.

  • Hi,

    I am not sure which document you are referring, but the u-boot debug procedure shows how to catch the processor at the very early stages of the system initialization and the video even shows how to halt the processor after a reset, which seems what you want to do. It obviously describes the procedure using the features, project source code and the binaries from u-boot, which we know for sure allows a complete source-code debugging.

    In this case, the same concepts and CCS options are applicable to the BSP code and you should have a similar capability of halting and single-stepping the core at the very early stages of the boot. All in all, the XDS emulator can obtain complete low-level control over the target core. The big question mark is if source-code debugging will be available, as it is dependent on the type of binary and debug symbols generated by the tools used to build the BSP.

    The Linux debug procedure is at a later stage in the initialization (when u-boot is already long gone) and therefore seems a lot more high-level for you.

    Hope this helps,

    Rafael

  • Hello,

    I guess i expressed myself a bit wrong way :)

    It feels a bit wrong for me to have the bootloaders (xloader & u-boot) taken from the Linux BSP (compiled with GNU toolchain) and then kernel image itself from the WinCE BSP (compiled with MS toolchain). Also having the binaries in different format (ELF for bootloaders vs kernel in COFF).

    But I guess that's the life is currently and nothing we can do about it.

    What comes to ELF format bootloaders, these i managed to debug properly while ago, set breakpoints, run-to and all other fancy features and CCS works the most excellent manner there. Also modifying hardware registries etc. Everything works like a charm. Now if it would support COFF (or any other MS binary format) for debugging, it would be the perfect tool. :)

    But, I keep searching. There has to be a way to use JTAG with binaries created with MS toolchains :)

  • Hi,

    Thanks for the clarification; I think you are very well aware of the initial debug procedure.

    Regarding u-boot loading WinCE, I know it feels strange but, all in all, u-boot simply loads raw binary code to the memory (it could be Linux or WinCE, as binaries are bit streams) and points to its initial address. It obviously performs some hardware initialization (DDR, RS232, Ethernet, etc.) but that would be necessary in any case. In the case of Linux, it also passes parameters to its kernel (as if it was calling a function), which I don't know if WinCE kernel would accept them.

    Also, CCS supports COFF but it is in a format used by our code generation tools (the TI compiler set). In this case you could try to load a Microsoft COFF binary and see if the debugger is able to interpret it correctly. Not sure, I never tried. 

    You got me curious - I can't promise anything, but I would love to try it someday. Maybe some other developer was able to use this combination and could give some tips.  

    Regards,

    Rafael

  • Hello,

    well, in principle you are correct. It does not make absolutely no difference, where i load the kernel from. But when i take it from the commercial point of view, mixing toochains within one project scope (gcc toolchain for bootloaders and MS toolchain for CE kernel) most definitely turns into a nightmare. And explaining it to customer would be even bigger nightmare. I'd like to keep things simple and straightforward: one project, one toolchain (wherever possible).

    So, whenever someone figures out, how to debug bootloaders compiled with MS toolchains using XDS100 and having Pandaboard as target board, i would be very glad to know about it.

    And if i figure out something, i will definitely post it here.