I have a C6745 on a board designed at my company and am using a SD XDS100V2 emulator. I brought the system up and was able to connect, but had a problem getting the code loaded due to a mapping problem. Through making changes to map the code properly, I lost the ability to connect to the target and can not figure out where I broke the device driver. Reinstalled CCS 4.2.4 and created a new target and still get
Error connecting to the target:
(Error -1265 @ 0x0)
Device ID is not recognized or is not supported by driver. Confirm device and emulator configuration is correct, or update device driver.
(Release 5.0.429.0)
Thanks, Jerry