hi
Plz solve this
using ccs5 and dm6446evm +xds510 usb emulator
C64XP_0: Error connecting to the target: Error 0x80000260/-1137 Fatal Error during: Execution, Initialization, OCS, It appears that the target is being held in reset. This may be due to Wait-In-Reset (WIR) configuration set by the EMU 0/1 pin settings. If this is the case, press Cancel and disconnect all connected devices to attempt to clear the WIR configuration. If this is a multi-core system, the master CPU or ICEPick may not be releasing the target from reset. Please check your configuration and/or your GEL files to ensure that nothing is blocking the target from being released from reset.
thanks
kailash