Other Parts Discussed in Thread: TMS320C6678
Hi,
I am using a TMS320C6678 eval board with Blackhawk XDS560v2-USB Mezzanine Emulator. Previously I was running CCS V5.1 on a 32-bit Windows XP machine, and launching the target configuration usually take a very short time. However, now that I have ported everything to a 64-bit Windows 7 machine, the time needed to fully launch a target configuration file takes approximately 10minutes. The symptoms that I observed is the progress bar will load smoothly till 99%, and at 99% it will get stucked for about 10minutes before all the cores can be seen on the debug screen. However, the time taken to connect to the cores as well as the time taken to load the program in seems to be normal. Is there any solutions to this or any settings that I might have forgotten to tweak after changing the machine? Will appreciate if someone can help. Thank you!