Other Parts Discussed in Thread: TM4C129XNCZAD
Hi,
I am trying to burn UBL for Davinci DM368 based IP camera from Appro(DM368IPNC-MT5) using CCS 5.2.1. I am using gel file (gel_ ipnc_dm36x_1.0.0.gel), provided from Appro. (Userguide recommend CCS version 3.3 )
I have setup "target configuration" and successfully connected with target but when I load any program I found following error messages regarding breakpoints. I do not have single breakpoint in my code. Please help me to resolve this issue.
-------------------------------------------
ARM9: Breakpoint Manager: Retrying with a AET breakpoint
ARM9: Trouble Setting Breakpoint with the Action "Process CIO" at 0x8e0097f0: Error 0x00000008/-1066 Error during: Break Point, Cannot set/verify breakpoint at 0x8E0097F0
ARM9: Breakpoint Manager: Retrying with a AET breakpoint
ARM9: Trouble Setting Breakpoint with the Action "Terminate Program Execution" at 0x8e009c18: Error 0x00000008/-1066 Error during: Break Point, Cannot set/verify breakpoint at 0x8E009C18
ARM9: Trouble Setting Breakpoint with the Action "Finish Auto Run" at 0x8e004604: Error 0x00000008/-1066 Error during: Break Point, Cannot set/verify breakpoint at 0x8E004604
Regards,
--HK