Other Parts Discussed in Thread: CONTROLSUITE, BOOSTXL-C2KLED
Working with the C2000 LaunchPad and LED BoosterPack Eval Kit, I tried to load the LED_Boost_PC program into CCS and got the message: "LED_Boost_PC compiler definition not available. Contact support." This same message comes up when trying to load the capacitive touch app code. Therefore, I can't load the flash on the LaunchPad and run the program. How do I update CCS to include this compiler definition.
Also, the LED control GUI loads fine on my PC and comes up, but it can't find the board (COM port is set. It finds that fine.). It is looking for a .a00 file extension.
So in general, the C2000 LaunchPad and LED BoosterPack is dead in the water. Help.
John Wolf : johnwolf.lobo@gmail.com