In CCS5 if I change a build property of a source file, for example optimisation level, then in project explorer the icon next to the file name becomes impaled by a golf tee. If I set the optimisation level back the golf tee is still there. If I restore defaults then the golf tee is still there.
(A) How do I get rid of the golf tee?
(B) How do I find out which of the many properties may not set at project default?
Regards --- Roger