Other Parts Discussed in Thread: TMS570LS20216, TMS570LS3137
Hi,
CCS 5.2.1.00018: CGT 5.0.1: TMX570LS3137B PGE001: JTAG Spectrum Digital XDS510USB Emulator
I am experiencing strange behaviour when running an image built with CGT 5.0.1 as opposed to the very same source built with CGT 4.7.1.
For a program built with CGT 5.0.1, under JTAG debug control, following power-on, the program will run from address zero. Something then causes a reset (which could well be my fault). However, the strange behaviour is that I cannot then run nor single step the program. The program counter remains fixed at zero.
For a program built under CGT 4.7.1, I do not get the reset. I have not witnessed a frozen program counter under CGT 4.7.1 over the many months I have been using it.
I am investigating the reason for reset independently, but am very keen to know what might cause the program counter to freeze under JTAG debug control.
Regards, Tony.