I'm a hobby user and just received my Stellaris LP's. I already have CCS v5 installed, but it only has the MSP430 tools and the 16KB limited license.
Do I need to have two versions of CCS installed to support the different licensing models? I tried running an install on my current location to add Stellaris support, but the licensing options are "Code Size Limited" and Free License for Stellaris. I can't choose both. I found an old thread suggesting this would be possible in 5.1, but that doesn't seem to be the case.
Just trying to figure out what the best route is before I run another ~3GB installation of CCS.