Hi All,
I was searching for a stream C I/O library to support sophisticated console over UART.
Referring following links understood that possible to port the RTS library for user defined device
1) Referring Chaper 8 in C/C++ User manual( http://www.ti.com/lit/ug/spru187u/spru187u.pdf)
2) User defined C I/O app note (http://www.ti.com/lit/an/spra861/spra861.pdf)
Is there reference Low level functional I/O implementation available for TI device?
Looking for the middle layer to glue high level I/O functions & UART HAL.
Regards
Vinoth