Hello,
We have an old test station here that recently failed. It was running CCS v2.21, Flashburn 2.5, and a Spectrum Digital JTAG emulator for the c5x series DSPs. We must have updated it to that version from the original media, which we have two copies: v2.0 and v2.1. The drivers require a minimum of v2.21 to work. We also have a 3.1 copy, that is fine for the drivers but our Flashburn install requires a 2.x version of CCS.
Is there a download link where we can update to v2.21?