CCS4.2.4 is installed in ProgramFiles/Texas Intruments folder in windows 7 machine. I am trying to build the project but it shows the message as cannot build the resources.
Problems occurred building the selected resources.
Errors running builder "Generated Makefile Builder" on project pa_i14_evmda830.
Cannot create file because existing file of wrong type exists: T:\pa\f\s19\i14\evmda830\Release.
Also attaching the log file from C:\Users\a0271801\.TI-trace
Regards
Asheesh
M 16:10:01:449 | Trace Factory: Calling CreateTraceFactory
M 16:10:01:449 | Trace Factory: CreateTraceFactory pStaticFactory=0x1c4bef20 refcount=1
M 16:10:01:449 | Trace Factory: calling CreateChannelServer m_channelServer=0x0
M 16:10:01:449 | Trace Factory: Reusing environment from previous session.
M 16:10:01:449 | Trace Factory: CreateChannelServer - connect existing
E 16:10:01:464 | Trace Factory: Channel server creation failed.
M 16:10:01:496 | Trace Factory: calling CreateChannelServer m_channelServer=0x0
M 16:10:01:496 | Trace Factory: Reusing environment from previous session.
M 16:10:01:496 | Trace Factory: CreateChannelServer - connect existing
E 16:10:01:496 | Trace Factory: Channel server creation failed.