I want to create emulation for C66 on my hardware board but I have a serious space constraints, hence I was thinking of using XDS100 which uses 14-pins header instead of 60-pin header for XDS560.
I would like to know what is the difference between XDS100, XDS510, XDS560.
XDS100 seems to consist of the 5 JTAG signals and EMU0:1. XDS560 seems to consists of the 5 JTAG signals and EMU0:18.
What is the difference between EMU and JTAG signals? Is it only a speed improvement? XDS560 will be faster than XDS100 due to the presence of the extra EMU signal to pass data.
If I uses XDS100, what will I not be able to do compared to XDS560? Can I still program the C66, step through the code, etc.