Other Parts Discussed in Thread: SYSBIOS
Hey Folks,
I'm working on a team that is currently designing a product based on the OMAP L138. Most of the work we've done so far was algorithmic and based on the C674x. All our development and debugging so far were done using Windows-compatible tools provided by TI. We just started work on the higher level system code that runs on the ARM and communication between the ARM and C674x and discovered that all the tools for the ARM are only available for Linux environments.
We're thinking of migrating all of our development for the C674x and the ARM to Linux to save the hassle of switching between the two environments. Does anyone have any experience doing all their development for C674x on Linux? A few particulars about our requirements (just being a little cautious and asking a few obvious questions.)
- Can we use the XDS100v2 and XDS510 emulators on Linux? If so, I'm assuming the emulators can be used to download and debug code.
- Are there any differences in debugging features between CCS on Windows and CCS on Linux?
- If we move to CCS on Linux and its related tools will this require any changes to the currently functional C674x code.
- Does moving to Linux pose any issues for SYSBIOS?
Any guidance is much appreciated.
Regards,
Dinesh