This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Concerto 32 bit code state setting

Under Project\Properties\C/C++ General\Settings\Processor Options

There is a "Designate code state, 16-bit (thumb) or 32-bit (--code_state)" setting that can select 32 or 16. I'm assuming the 32 bit would be an enhanced performance. However when applying and then building the project a warning states:

"--code_state=32 is invalid for Cortex-M (ignored)"

Is this an issue with CCS 5.2 or is it a limitation of the F28M35H52? We are using the control card TMXCNCDH52C1 and the version of CCS5 is

Version: 5.2.0.00069