I have been using MyEclipse development environment (currently version 10.0) for several years now for Java development and I now have a need to use Code Composer Studio 5 (CCS5). One of the options is to install the CCS5 plugins into an existing Eclipse installation (which I prefer to do), however, when I select the option and point to the Existing Eclipse Location, I get an error saying "There is no eclipse executable found in C:\Users\<myName>\AppData\Local\MyEclipse Please choose a valid location". This path is the proper one and the executable is named myeclipse.exe. It is true that it is not really an 'eclipse' installation however I was wondering if it is possible to install the plugins into my existing MyEclipse environment? and if so, could you please explain how? If it is not possible using the installation program, is it possible to successfully install the plugins from the installation image. Any help would be appreciated.