This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Procedure for setting breakpoints on the iCont side of DM816x

Kindly let me the procedure for setting breakpoints on the iCont side of DM816x EVM  for the files that are built with -g option to enable stepping inside the iCont code.

Also, M3 host is built in "Debug" mode.

As of now, I am able to set breakpoints & debug only on the M3 side.

Appreciate if the procedure is provided at the earliest as I am stuck at this point and not able to proceed futher.

Thanks..