Other Parts Discussed in Thread: UNIFLASH
Hello,
I'm trying to use UniFlash to program both cores on a Concerto, but right now I'm concentrating on the M3 core. After a lot of experimentation I've found that the GUI works if I go to the Program menu, click on Load Program and then navigate to my OUT file.
But if I click on "Programs" in the main view, add the same OUT file to the program list and click the Program button, it doesn't work. I see a pop up window telling me the file is being loaded, that stays on the screen for a moment, and then it disappears and the console window says "Programs Loading Finished". But the program wasn't really loaded. I never saw the progress bar moving and I didn't see any messages about Flash being erased, etc. When I cycled power on my board I could tell the program wasn't running.
What's the difference between these two programming methods? Why does one work and the other doesn't?
I'm also trying to program from the command line and that isn't working. Maybe the command line is basically the same as using the main view (which doesn't work in the GUI either).
Thanks,
Joel