Other Parts Discussed in Thread: TMS320C6678
dear all
There is a 6678 and XDS100V1 in my PCB. when I want to load .out file to 6678. there is a error:
C66xx_1: Trouble Writing Register PC: (Error -1176 @ 0xD720) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.0.569.0)
bisides. We can not connect to core0,When we want to connect to core 0.the problem is:
C66xx_0: Error connecting to the target: (Error -1180 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 5.0.569.0)
I have checked to power supply and clock. the resetstate pin is high. and the gel file is loaded to target configure file.
C66xx_0: GEL Output: Setup_Memory_Map...
C66xx_0: GEL Output: Setup_Memory_Map... Done.
C66xx_1: GEL Output: Setup_Memory_Map...
C66xx_1: GEL Output: Setup_Memory_Map... Done.
C66xx_2: GEL Output: Setup_Memory_Map...
C66xx_2: GEL Output: Setup_Memory_Map... Done.
C66xx_3: GEL Output: Setup_Memory_Map...
C66xx_3: GEL Output: Setup_Memory_Map... Done.
C66xx_4: GEL Output: Setup_Memory_Map...
C66xx_4: GEL Output: Setup_Memory_Map... Done.
C66xx_5: GEL Output: Setup_Memory_Map...
C66xx_5: GEL Output: Setup_Memory_Map... Done.
C66xx_6: GEL Output: Setup_Memory_Map...
C66xx_6: GEL Output: Setup_Memory_Map... Done.
C66xx_7: GEL Output: Setup_Memory_Map...
C66xx_7: GEL Output: Setup_Memory_Map... Done.
C66xx_1: GEL Output:
what is the problem? any advice will be nice.