Hello everyone,
First of all thank you very much for your great help.Finally i linked the files successfully.
with regards,
Ritesh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello everyone,
First of all thank you very much for your great help.Finally i linked the files successfully.
with regards,
Ritesh
I think he is referring to this thread. -George
Hello Sir,
I have to read text file from SD card. I have written simple file handling code of file handling to read text file. This code works fine in Turbo C++ compiler. For executing this code in CCSv4, I have include functions like initialization of USBSTK5515 and SD card. This gives me error as below:
In Problem Window:
"C:/Program Files (x86)/Texas Instruments/ccsv4/emulation/boards/usbstk5515_v1/lib/usbstk5515bsl.lib<usbst k5515.obj>" has a Tag_Memory_Model attribute value of "2" that is different than one previously seen ("3"); combining incompatible files text line 0 1351948471265 456
In Console Window:
fatal error: file "C:/Program Files (x86)/TexasInstruments/ccsv4/emulation/boards/usbstk5515_v1/lib/usbstk5515bsl.lib<usbstk5515.obj>" has a Tag_Memory_Model attribute value of "2" that is different than one previously seen ("3"); combining incompatible files
>> Compilation failure
C:\Program Files (x86)\Texas Instruments\ccsv4\utils\gmake\gmake: *** [text.out] Error 1
C:\Program Files (x86)\Texas Instruments\ccsv4\utils\gmake\gmake: Target `all' not remade because of errors.
Build complete for project text
Please help me correct this issue.
Thank you!
Regards,
Ritesh