This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSv5.1.1: compiler issue?

Hi,

I am using CCS 5.1.1 under linux and I am experimenting the following issue.

This is an excerpt of the map file:

text   (code area)

                  ..................

                  0c1a6b20    00000010                                                  : PLT_bcp.oe66 ($Tramp$S$$PLT_Bcp_getUlTxQue)
                  0c1a6b30    00000010     --HOLE-- [fill = 0]

.prachBuffers  (data area)
*          0    0c1a6b30    0002b000     UNINITIALIZED
                  0c1a6b30    0001e000     phy_phy_phy_ul_debug_e66.ae66 : PHY_TSK_prachReceiver.oe66 (.prachBuffers)
                  0c1c4b30    0000c000                                                  : PHY_UL_prachDecimationFilter.oe66 (.prachBuffers)

It can be seen that an hole is inserted at 0x0c1a6b30, probably to get aligned, but actually there is no hole, because data area start at 0x0c1a6b30 too, overlapping.

Is the above a compiler bug?

Any feedback is welcome.

thanks

Regards

Stefano