Other Parts Discussed in Thread: CCSTUDIO
I have a problem with launching a project in Code Composer studio Version 5.2.0.00069.
I use the evaluation kit Stellaris EKS-LM4F232.
When I press the debug button it starts initializing and downloading the code, but it doesn’t work.
In the Console it writes:
CORTEX_M4_0: GEL Output:
Memory Map Initialization Complete
And then it stops. In the right side the green bar is still working and the system writes:
Launching hello (100%).
The situation is the same with evaluating connected or not.
But the system locks, I can’t close down the process, even with the task manager. A process named ccstudio.exe can’t be killed. That means that I have to reboot the PC before I can start code composer studio up again.
I have reinstalled everything’s and it works one time, but after a new debug start the behavior is the same, the system locks when I start debugging.
I have to mention that I have a laptop where the same installation works, but it is an old machine which is very slow, and I share this with others.
Does anyone have similar problems and what was the solution?
Best regards,
Bent