Other Parts Discussed in Thread: MSP430F5529
Which MAC address is valid ? I have tried both the hard wired network and the wireless and neither
seems to work. Everything else seems to work. Unless I can resolve this, I can't upgrade to a paid
license which I would like to do. I am doing this for personal projects so I want the cheapest solution
possible for large code projects for MSP430F5529 devices.
lo: flags=73<UP,LOOPBACK,RUNNING> mtu 16436
inet 127.0.0.1 netmask 255.0.0.0
loop txqueuelen 0 (Local Loopback)
RX packets 43312 bytes 3808636 (3.6 MiB)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 43312 bytes 3808636 (3.6 MiB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
p5p1: flags=4099<UP,BROADCAST,MULTICAST> mtu 1500
ether 14:da:e9:cf:fc:9d txqueuelen 1000 (Ethernet)
RX packets 0 bytes 0 (0.0 B)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 0 bytes 0 (0.0 B)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
wlan0: flags=4163<UP,BROADCAST,RUNNING,MULTICAST> mtu 1500
inet deleted for privacy netmask 255.255.255.0 broadcast 10.0.0.255
inet6 deleted for privacy prefixlen 64 scopeid 0x20<link>
ether 74:2f:68:9c:a6:65 txqueuelen 1000 (Ethernet)
RX packets 454275 bytes 267806346 (255.4 MiB)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 326591 bytes 42787979 (40.8 MiB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0