This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Fail to get connection with emulator

Hi,

I have CCS5.2 running in Ubuntu 12.04. When I try to hook up the XDS560 emulator and test the connection, I get the following error.

 

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 560-class product.
This utility will load the program 'bh560v2u.out'.
E_RPCENV_IO_ERROR(-6) No connection: open failed: code 19
Download failed for file /opt/ti/ccsv5/ccs_base/common/uscif/./././././xds560v2.out

An error occurred while soft opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.

The explanation is:
An attempt to access the named emulator via USCIF ECOM has failed.

 

So can someone tell me what is wrong?

Thanks,
Charles