Hello, I am trying to program my target and I keep getting the error shown in the subject. and it does not program after I click "yes"
I sometimes get this error about having to cdt consoles open, how do i close them and get to program?
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello, I am trying to program my target and I keep getting the error shown in the subject. and it does not program after I click "yes"
I sometimes get this error about having to cdt consoles open, how do i close them and get to program?
thanks
Hi Andrew,
as I am sure you are aware you should be able to debug if you say yes to closing whatever debug session may be open .. ie when you get that message.
Some things I recommend trying/checking as a first step
- do you have any hidden files in your project tree? Ie did you .project or metatdata etc become hidden files? Try making them unhidden.
- try importing the project to a fresh workspace using Project->Import existing CCS/Eclipse Project
- another thing would be to try the latest release of CCS
Please keep us informed.
Best Regards,
Lisa
Hello,
I was wondering if here was found a solution. I have the same problem with one specific project in my workspace. I tried to options Lisa mentioned but it didn't help.
I tried:
- a new workspace
- there are no hidden files in my directory
- I updated the compiler from 4.1.2 to 4.1.3
I am running CCS v5.1. I have it only with one project, the other projects I can start en stop debugging but if i do that to the "problem project" i have to restart CCS before I can start a new debugsession.
I here a solution for this problem?
Best Regards,
Jeroen
Hi Lisa,
No, I'm sorry. I can't sent the project because of company secrets.
I tried an example project, that is working fine. Do you have some suggestions where i can look for the problem or the difference between the projects?
Best Regards,
Jeroen Begeer
Hi Jeroen,
till today I had the same problems with CCS5.1.
The following steps solved the problems I had:
I did it this way and till now everythings works fine.
Best regards, Tagi
i keep having this problem reoccur, then I create a new workspace which has worked, but not consistently.
following the instructions above did not help: during copy do I overwrite .settings and other project files? i did and it did not work
Likely something I am doing wrong but what please help this is taking a lot of time. ccs v5.2.1
Hi Andrew,
would you please create a new thread with your problem, logs and further details. This will help us get you the best support.
Best Regards,
Lisa
Hi Andrew,
In my case i noticed that if i copied the .metadata folder of the new working workspace( which I generated when I followed the steps from Tagi) to the not working workspace, I had to add my projects again but then the projects worked fine again.
Maybe you have something about this information.
Best regards,
Jeroen